Diodes Incorporated (Diodes) (Nasdaq: DIOD) addresses the increase in automotive computing capabilities and its accompanying high-speed interfacing with the new DIODES PI3DBS16222Q. This four-channel differential exchange switch provides a performance-optimized multiplexing solution and is targeted for automotive infotainment, telematics, SATA 3.0, SAS 3.0, and ADAS systems.
The automotive-compliant PI3DBS16222Q enables 2x2 differential multiplexing at speeds of 20Gbps, and supports USB 3.2 Gen 2, PCI Express 4.0, and 10GBASE-KR standards. The device leverages a proprietary design technique, enhancing its dynamic electrical characteristics. This delivers low insertion-loss
(-2.0dB at 10GHz typical) and crosstalk (-17dB at 10GHz typical) figures, ensuring high signal-integrity levels. In addition, the device attains a 10ps bit-to-bit skew, and a low return-loss.
The PI3DBS16222Q high-speed, multi-channel exchange switch from Diodes is AEC-Q100 Grade 2 qualified, manufactured in IATF 16949 certified facilities, and supports PPAP documentation. It is supplied in a compact 2.5mm x 4.5mm TQFN-30L (ZL30) package, and it is available at $2.50 in 3,500 piece quantities.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
© 2023 Copyright Diodes Incorporated. All Rights Reserved.
Company Contact: Investor Relations Contact:
Diodes Incorporated Shelton Group
Emily Yang Leanne K. Sievers
SVP, Worldwide Sales and Marketing President
P: 972-987-3900 P: 949-224-3874
Contact Us E: lsievers@sheltongroup.com