Diodes Incorporated — Analog and discrete power solutions

8-Pin Miniature Logic Devices from Diodes Incorporated Boost Battery Life

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today extended its advanced ultra-low power CMOS logic family with the introduction of dual-gate devices in the miniature, leadless 8-pin DFN1210 package. The latest 74AUP2G logic devices help extend battery cell life in a variety of super slim, next-generation portable products, such as smart phones and tablets, by supporting low-voltage, low-power system design.

Operating over a 0.8V to 3.6V supply voltage range, these new parts support extremely low system voltages while delivering a standard ±4mA output. With quiescent current less than 0.9μA, static power consumption is low, while the typical CPD rating of 6pF at 3.6V reduces dynamic power consumption.

Seven dual gate logic functions are offered: AND, NAND, OR, NOR, XOR and a choice of two tri-state buffers. With a footprint of only 1.2mm x 1.0mm and a height of just 0.35mm, the DFN1210 format is one of the world's smallest 8-pin packages.

The miniature-packaged parts are designed to complement Diodes' previously released 74AUP2G 6-pin dual-gate and 74AUP1G single-gate advanced ultra-low power logic. Further information is available at www.diodes.com.

About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes' corporate headquarters and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes' wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes' website at www.diodes.com.

Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com

Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com