Diodes Incorporated (Nasdaq: DIOD) has introduced the PI7C9X3G808GP, a PCIe® 3.0 packet switch capable of delivering the elevated performance parameters mandated by modern data center, cloud computing, network-attached storage (NAS) and telecom infrastructure implementations. The packet switch supports 8-lane operation, accommodating 2-port, 3-port, 4-port, 5-port, and 8-port configurations. Cut-through, store and forward modes can all be utilized, with a packet forwarding latency of less than 150ns (typical) being supported.
The proprietary architecture employed in the PI7C9X3G808GP packet switch provides enhanced flexibility and performance. Multiple port / lane width combinations are available, as well as cross-domain end-point (CDEP) arrangements. Thanks to its CDEP capabilities, the PI7C9X3G808GP supports fan-out and dual-host connectivity.
The built-in PCIe 3.0 clock buffer allows for a reduction in the overall component count and helps to curb BOM costs. This integrated buffer is unique to the industry, because of its low-power operation. Three different reference clock options can be used: common, separate reference no spread (SRNS), and separate reference independent spread (SRIS). Multiple direct memory access (DMA) channels have been embedded into the switch, in order to make communication between host (or hosts) and connected end-points as efficient as possible.
Features include error-handling, advanced error reporting, and end-to-end data protection with error correction - key functionality in terms of reliability, availability, and serviceability (RAS). The advanced power management means that this switch is aligned with the most stringent energy-saving requirements. Hot-pluggable ports that are empty are kept in a low-power state until they are needed. Under full load conditions and 80°C junction temperature, the PI7C9X3G808GP will draw only 2.9W of power.
Diodes Incorporated’s PI7C9X3G808GP is supplied in a high-performance flip-chip package, with 196-ball BGA format. It has dimensions of 15mm x 15mm. This next generation packet switch has a unit price of $20.13 in 1000 piece quantities.
PCI Express® and PCIe® are trademarks or registered trademarks and/or service marks of PCI-SIG Corporation.
##
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 31 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.Diodes.com.
Company Contact: Investor Relations Contact:
Diodes Incorporated Shelton Group
Emily Yang Leanne K. Sievers
VP, Worldwide Sales and Marketing EVP, Investor Relations
P: 972-987-3900 P: 949-224-3874