CORRECTION...by Diodes Incorporated
PLANO, Texas--(BUSINESS WIRE)-- Second paragraph, second sentence of release dated September 30, 2022, should read: "Its low input noise density (9.5nV/√Hz) and 0.8µVpp low frequency noise..." (instead of 7.5 nV/√Hz and adding the word low before frequency).
The updated release reads:
AUTOMOTIVE-COMPLIANT PRECISION OP-AMPS FROM DIODES INCORPORATED OFFER WIDE DYNAMIC RANGE AND LOW NOISE OPERATION
Diodes Incorporated (Diodes) (Nasdaq: DIOD) is addressing the need for advanced signal conditioning in modern automotive designs by introducing two precision operational amplifiers (op-amps) aimed at different signal frequency scenarios. The low signal-to-noise ratio characteristics of the DIODES™ AS2376Q mean it is optimized for high frequency usage, such as in on-board chargers (OBCs), DC-DC converters, battery management system (BMS) implementations, pumps, airbags, position sensors and occupancy detection systems. The minimal quiescent current exhibited by DIODES™ AS2333Q, launched in August, make it highly suited to addressing functions that continue even when the vehicle is inactive.
A 5.5MHz bandwidth enables the AS2376Q op-amp to handle 50kHz signals without significant loss of signal accuracy. Its low input noise density (9.5nV/√Hz) and 0.8µVpp low frequency noise, coupled with rail-rail output, result in enhanced signal integrity. With 5μV (typical) offset voltage, the AS2376Q supports a wide dynamic range. Supply voltages from 2.2V to 5.5V are accepted, enabling greater design-in flexibility.
The AS2333Q op-amp has a quiescent current of just 12μA on each amplifier channel that allows it to be used in systems that have to remain live at all times. Excellent common-mode rejection ratio (CMRR) across its rail-rail input range coupled with near-zero drift over time and temperature provide long-term signal accuracy in wide common-mode rail precision applications. Its 1.8V to 5.5V supply voltage enables it to operate from 3.3V and 5V automotive rails.
The AS2376Q and AS2333Q are supplied in the SO-8 package. These devices are available at unit pricings of $0.93 and $1.56 respectively in 1000 piece quantities. Both are qualified to AEC-Q100 Grade 1, are manufactured in IATF 16949 certified facilities, and support PPAP documentation.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
DIODES is a trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
Contacts
Company Contact:
Diodes Incorporated
Emily Yang
SVP, Worldwide Sales and Marketing
P: 972-987-3900
Contact Us
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
President
P: 949-224-3874
E: lsievers@sheltongroup.com
Source: Diodes Incorporated (P)