Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today announced the AL1663 and AL1663R. These single-stage dimmable LED controllers support fly-back and buck-boost topologies in order to provide primary-side regulation that achieves an accurate constant-current output without requiring opto-couplers and secondary control circuitry. Operating at up to 150W and featuring multiple dimming options, these controllers provide versatile and cost-effective drivers for LED backlighting, smart LED lighting and general-purpose dimmable LED lamps.
High efficiency and low EMI result from operation in boundary-conduction mode (BCM) with valley-switching control, which further ensures the AL1663 and AL1663R maintain high power-factors with low total harmonic distortion under universal input-voltage conditions. The use of primary-side regulation simplifies design and lowers total BOM component count and cost. The AL1663 and AL1663R are also characterized by low start-up current and low operating current, and integrate multiple protection features including over-voltage, short-circuit, over current and over-temperature.
Analog and digital dimming modes are supported: the AL1663R has a single dimming pin that will accept either an analog signal between 0.3V and 2.4V DC or a digital PWM input when connected with a suitable input capacitor of several hundred nF. The AL1663 offers an additional digital dimming input pin that can accept a high-frequency PWM signal and provides built-in PWM-to-DC conversion. The AL1663 and AL1663R are both offered in SO-8 packages.
For further information, visit the Company’s website at www.diodes.com.
###
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com