Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, and Weltrend Semiconductor Inc., a leader in USB Type-C™ Power Delivery (PD) controllers, today announced a joint reference design for a 27W, Class A charger that is one of the industry’s first chargers to support Qualcomm® Quick Charge™ 4 specification for the fast charging of mobile devices.
Quick Charge 4 is the latest fast-charging specification from Qualcomm Technologies, Inc., a subsidiary of Qualcomm Incorporated, offering up to 20% faster charging, up to 30% greater efficiency, and running 5% cooler when compared to Quick Charge 3.0. Quick Charge 4 also supports USB PD and PPS (programmable power supply), helping to standardize the capabilities of adaptors using these technologies, while being designed to deliver headline-making charging performance that provides five hours of talk time from just five minutes of charging, along with comprehensive safety features.
“Diodes’ key corporate strength is rooted in its integrated device manufacturing (IDM) operations model. Leveraging our vertical integration manufacturing strength in conjunction with a platform solution approach provides the relevant active components required for target systems, especially as Diodes has a well-established business in providing primary- and secondary-side power regulation products for chargers and power adapter applications”, said Ernest Lin, Division Manager, AC-DC Power and Lighting Division. “Diodes recognized Weltrend’s core competency in MCU-based power management applications and its established market position in protocol decoding products for quick charging, which made for a logical partnership for developing a reference design to meet the demanding requirements of the Qualcomm Quick Charge 4 specification.”
The reference design uses Diodes’ AP3302 peak-current control, quasi-resonant (QR) PWM controller, which is optimized for high performance, low standby power and cost-effective offline flyback conversion, and its APR345 secondary-side MOSFET synchronous rectification driver that directly supports CCM, DCM and QR flyback topologies. Weltrend provides the highly integrated WT6615F programmable protocol decoder that supports the latest programmable power supply specification for Quick Charge protocols and USB PD, and consequently fully implements all the requirements of the Quick Charge 4 specification.
Tony Lin, Executive Assistant to the CEO and Acting VP of Marketing at Weltrend, said, “Working closely with Qualcomm Technologies, our expertise lies in understanding fast charge protocols and we are excited to be one of the first in our industry to provide a Quick Charge 4 compatible chipset. The joint development of this 27W Quick Charge 4 Class A reference design with Diodes provides a cost-effective, ready-to-go charger design that enables a rapid time-to-market solution for our mutual customer bases”.
Weltrend’s WT6615F Qualcomm Quick Charge 4 Controller is certified by GRL. The reference design supports Quick Charge 4 Class A (18-27W) and also provides optional Quick Charge 2.0 and Quick Charge 3.0 compliance to support the Quick Charge 4+ program. It provides support for USB PD 3.0 and PPS, including PDO at 5V and 9V, ADPO from 3V to 11V in 20mV steps, and current from 0A to 3A in 50mA steps. Its safety management capability provides monitoring of voltage, current, and temperature, with reporting and protection features. The charger design supports low standby current consumption and meets Energy Star DOE VI and CoC Tier II efficiency requirements.
Further information is available at www.diodes.com.
Qualcomm is a trademark of Qualcomm Incorporated, registered in the United States and other countries. Quick Charge is a trademark of Qualcomm Incorporated.
Qualcomm Quick Charge is a product of Qualcomm Technologies, Inc.
USB Type-C and USB-C are registered trademarks of the USB Implementers Forum.