Diodes Incorporated (Diodes) (Nasdaq: DIOD) announces its SDT2U30CP3 (30V/2A), SDT2U40CP3 (40V/2A), and SDT2U60CP3 (60V/2A) achieve the industry’s highest current densities in their class with low forward voltage drop and thermal resistance addressing design challenges for smaller and more efficient portable, mobile, and wearable devices. This series of innovative high-current trench Schottky rectifiers are housed in a chip-scale package (CSP) that occupies only 0.84mm² board space. They can be employed for a variety of different purposes, serving as blocking or reverse-polarity protection diodes, boost diodes, and switching diodes.
The trio are the first ever 2A trench Schottky rectifiers to be designed into the X3-DSN1406-2 package, making these the industry’s smallest in their class. Compared with similar SMB packaged devices, they take up a mere 3.4% of the PCB area. These ultra-thin CSPs, featuring a typical profile of 0.25mm, also shorten thermal paths. This results in enhanced power dissipation, ultimately reducing thermal bill-of-materials costs and significantly increasing overall system reliability.
Their ultra-low forward voltage performance, typically 480mV (580mV for the SDT2U60CP3), minimizes power losses, enabling the design of higher efficiency systems. They have superior avalanche capability compared to other products in the same range, ensuring robustness in extreme operating conditions, such as transient voltages, and providing an extra layer of reliability. Furthermore, these devices are totally lead-free and fully compliant with RoHS 3.0 standards, contributing to environmentally responsible designs.
The SDT2U30CP3, SDT2U40CP3, and SDT2U60CP3 rectifiers are available at unit price of $0.16, $0.17, and $0.19 respectively in 2,500 piece quantities.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the automotive, industrial, computing, consumer electronics, and communications markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
© 2024 Diodes Incorporated. All Rights Reserved.
Company Contact:
Gurmeet Dhaliwal
Director, Investor Relations & Corporate Marketing
Diodes Incorporated
+1 408-232-9003