Diodes Incorporated — Analog and discrete power solutions

Multi-Channel Load Sink Driver from Diodes Incorporated Consumes 12x Less Power than Industry-Standard Part

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the ULN2003V12 and ULN2003F12. The ULN2003V12 is a 7-channel relay and inductive load sink driver that consumes 12 times less power while offering a direct replacement to the industry-standard device. The ULN2003F12 is a 4-channel version, which provides a smaller footprint when fewer output channels are required, such as when driving low-voltage stepper motors. Target end-markets for these devices include domestic appliances like washing machines and dishwashers.

The ULN2003V12 and ULN2003F12 both support 3.3V to 5V CMOS logic inputs, making them compatible with a wide range of microcontrollers and logic devices. They also both integrate an input RC snubber circuit, which improves performance in noisy operating conditions, and an internal input stage pull-down resistor to simplify the use of tri-state input logic. The use of low-output impedance drivers minimizes on-chip power dissipation while still supporting output pull-up voltages up to 20V. The devices feature low, 25μA/channel supply current and outstanding ESD performance of 4kV HBM, making them suitable for industrial applications.

A key feature of the ULN2003V12 and ULN2003F12 devices is that each output is connected in a common-cathode configuration via internal freewheeling diodes to the COM pin. This provides an increased current sink capability by combining several adjacent channels in parallel. For example, under typical conditions the ULN2003V12 can handle a 1A load current when all seven channels are connected in parallel. Miniaturized packages help reduce board space requirements, with the ULN2003V12 available in SO-16 and TSSOP-16 packages, while the ULN2003F12 is offered in the U-DFN3030-10 package. Further information is available at www.diodes.com.

About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes' corporate headquarters and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes' wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information, including SEC filings, visit Diodes' website at www.diodes.com.

Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com

Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com