Diodes Incorporated — Analog and discrete power solutions

Pericom Expands Support for High Speed Connectivity

Newest Products Benefit Networking, Embedded, Server, and Mobility Applications

Pericom Semiconductor Corporation (now a part of Diodes Incorporated) (NASDAQ: DIOD), a leading supplier of serial high-speed switching, connectivity, signal-integrity and timing solutions, today announced expanded product families in support of next generation networking, embedded, mobility, and server platforms. Pericom will display these products at IDF, Moscone Center, San Francisco, CA, August 16-18, 2016 at Booth # 620.

Networking control plane processors and embedded processor applications often need PCI Express® (PCIe®) port expansion technology to handle the newest and most complex data plane and embedded multi-function designs. Pericom has added four new packet switches based on the PCIe 2.0 specification, ranging from 8 port/8 lanes to 16 port/24 lanes. These latest additions provide advanced power saving and management, DMA (Direct Memory Access), and are optimized to provide cost effective port expansion across a wide range of networking and embedded applications.

"As a PCI-SIG® member, Pericom holds an important role in the success of PCIe technology," said Al Yanes, PCI-SIG chairman and president. "The company's support of PCIe solutions helps the PCI Express ecosystem attain applicability within an increasing range of platforms in the market."
Many of the latest server and storage platforms utilize multiple high speed protocols, such as 10Gbps USB 3.1 and PCIe 3.0 technology at 8Gbps, 10GbE, and 12Gbps SAS3. Pericom has added two multi-protocol linear redriver ICs to its signal integrity solutions family that can handle all 3 protocols and meet link training and standards compliance specifications from 8Gbps to 12Gbps. The new parts offer flow through pinout, low power, and 2 or 8 fully independent user programmable channels of signal boost to extend high speed traces or cables in server and storage platforms.

Pericom is also the first to offer a fully linear 2 channel USB 3.1 redriver that supports both 10Gbps (USB 3.1 GEN2) and 5Gbps (USB 3.1 GEN1) speeds.

Additional new switch products for server and storage platforms include two I2C multiplexers (MUX) that offer 1:4 and 1:8 fan-out capability of the I2C bus, with any combination of downstream ports selectable. These parts add flexibility to I2C bus designs in more complex platforms where the I2C bus is also tasked to provide I/O functionality as well as legacy I2C control. A new 14bit SSD switch is ONFI3 compliant, optimized for supporting high capacity SSD memory modules through fast enable and select timing.

Moreover, five new PCIe 3.0 very low power clock generators and buffers offering user programmable slew rate and supporting x2/x4/x8 outputs, expand the timing product portfolio for server, storage, and embedded platforms.

"Pericom's new product roadmap continues to benefit our processor chipset partners," said Andy Tsong, division manager for Pericom products. "We enable and maximize the new features that are used by platform designers. For example, PCI Express technology continues to demand new timing, switching, conditioning, and routing solutions, and Pericom's focus and roadmaps support all of these necessary functions."

Product Part Numbers and Availability:

Samples and production quantities for most products are available now.

PCIe 2.0 Packet Switch products:

PI7C9X2G808PR - 8-port, 8-lane, PCIe 2.0 Packet Switch
PI7C9X2G912GP - 9-port, 12-lane, PCIe 2.0 Packet Switch
PI7C9X2G1616PR - 16-port, 16-lane, PCIe 2.0 Packet Switch
PI7C9X2G1224GP - 12-port, 24-lane, PCIe 2.0 Packet Switch

Switching products:

PI4MSD5V9546A - 4-Channel I2C /SMBus Bus Switch with RESET
PI4MSD5V9548A - 8-Channel I2C /SMBus Bus Switch with RESET
PI2SSD3212 - 1.35V/ 1.5V/1.8V 14 bit 2:1 SSD Switch

PCIe 3.0 1.8V Low Power HCSL Timing products:

PI6CG18201 - Clock Generator with 2 outputs and on-chip termination
PI6CG18401 - Clock Generator with 4 outputs and on-chip termination
PI6CG18801 - Clock Generator with 8 outputs and on-chip termination
PI6CB18800 - Clock Buffer with 8 outputs
PI6CB18801 - Clock Buffer with 8 outputs with on-chip termination
Recently announced USB 3.1, PCIe 3.0/10GbE/SAS3 Combo

ReDriver/Repeater products:

PI3EQX12908A - 8-Channel PCIe 3.0/10GbE/SAS3/SATA3 Combo Linear ReDriver
PI3EQX12902B - 2-Channel PCIe 3.0/10GbE/SAS3/SATA3 Combo Linear ReDriver
PI3EQX1002B - USB 3.1 Gen 2 Linear ReDriver / Repeater

Additional information and a volume pricing quote is available from Pericom worldwide sales, or by requesting a specific product price quote on www.diodes.com.

About Pericom:

Pericom Semiconductor Corporation enables serial connectivity with complete solutions for computing, communications and consumer market segments. Pericom's integrated circuits (IC) and frequency control products (FCP) provide the connectivity, timing, switching, bridging and signal conditioning of high-speed signals required by today's electronic applications. Pericom is based in Milpitas, California, with design centers and technical sales and support offices around the world. Pericom was acquired by Diodes Incorporated (NASDAQ: DIOD). Learn more at www.diodes.com.

About PCI-SIG

PCI-SIG is the consortium that owns and manages PCI™ specifications as open industry standards. The organization defines industry standard I/O (input/output) specifications consistent with the needs of its members. Currently, PCI-SIG is comprised of nearly 800 industry-leading member companies. To join PCI-SIG, and for a list of the Board of Directors, visit www.pcisig.com.

PCI Express®, PCIe®, PCI-SIG®, and PCI™ are trademarks or registered trademarks and/or service marks of PCI-SIG Corporation. All other trademarks are the property of their respective owners.