Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the DMN3027LFG 30V N-channel MOSFET. This device is designed as a switch to rapidly and safely discharge large bulk capacitors used on FPGA power rails. The latest FPGAs found in telecoms equipment, servers and data centers have multiple power rails that need to be correctly sequenced to safely power these systems up and down. Designers of high-reliability DC-DC power supplies can achieve this quickly and easily with this new MOSFET from Diodes.
The DMN3027LFG has an RDS(on) of 26mΩ at 4.5V, which is low enough to discharge a 15mF capacitor in
The DMN3027LFG is offered in a PowerDI®3333 package, which has a low thermal resistance from junction to exposed pad of <10°C/W enabling the dissipation of up to 3W. For further information, visit the Company’s website at www.diodes.com.
###
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
PowerDI is a registered trademark of Diodes Incorporated.