Diodes Incorporated

Active OR’ing Controller from Diodes Incorporated Increases Maximum Voltage to 200V for High-Reliability Power Systems

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today introduced the ZXGD3111N7. This active OR-ing MOSFET controller increases performance with a 200V maximum drain voltage and is targeted at power systems that use redundancy to achieve high reliability in telecom, data center and server applications. This increase in VDRAIN from the previously announced 40V ZXGD3108N8 allows this latest device to address requirements in 48V common rail systems where the outputs of two or more power supplies are OR’ed together in order to provide redundancy.

In addition to its 200V rating, which is twice that of its competitors, the ZXGD3111N7 has a low turn off threshold voltage with a tight tolerance of -5mV to -1mV. This improves stability under light load conditions when using low RDS(ON) MOSFETs, making this controller a class-leading solution that can deliver the highest efficiency and reliability over the entire load range.

The ZXGD3111N7 is designed to work with a FET to create an ideal diode that replaces the blocking diodes typically used in common rail designs. A 5A sink current capability allows fast discharge of the gates in the paralleled OR’ing MOSFETS and its quick www.diodes.com.

###

Company Contact:
Diodes Incorporated
Francis Tang
VP, Worldwide Discrete Products
P: 972-987-3900
E: pressinquiries@diodes.com

Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com

 

Related Files