Diodes Incorporated — Analog and discrete power solutions

Decoder IC from Diodes Incorporated is Compatible with Qualcomm Quick Charge 2.0 Protocol for Cell Phones

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the AP4370. This device is a decoder IC for the quick charging of cell phone, tablet and similar consumer products based on Qualcomm SoCs featuring its Quick Charge (QC) technology.

By ensuring compatibility with Qualcomm’s high-voltage dedicated charging port QC 2.0 protocol, this decoder provides a highly integrated and cost-effective solution for designers of chargers and adaptors that need to support the QC function. The AP4370 decodes different combinations of D+/D- signals generated by the portable device, producing V1/V2 outputs that can change either the controller’s voltage reference or voltage feedback divider resistor to achieve the required constant voltage/constant current control.

The AP4370 has an over-voltage discharge feature that protects a QC 2.0 connected device when it requests a lower output voltage by accelerating the output voltage decline during the transition. If a connected device is not QC 2.0 compatible, the decoder automatically provides a 5V output configuration. The AP4370 operates from a 5V to 12V with an ultra-low static current of just 90µA at 5V output. Requiring few external components and benefitting from small SOT26 or TSOT26 package options, this IC offers both board space and BOM cost savings. Further information is available at www.diodes.com.

###
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
Qualcomm is a trademark of Qualcomm Incorporated, registered in the United States and other countries. Quick Charge is a trademark of Qualcomm Incorporated

Related Files