Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the DSR8F600. This 600V 8A hyper-fast rectifier has been designed specifically for use as a boost diode for power-factor correction (PFC) and continuous conduction mode (CCM) applications. The target market is in switched-mode power supplies (SMPS) that need to deliver a high output, greater than 75W, in end-equipment such as flat-panel TVs, servers and telecoms systems, where new regulatory standards in Europe, the USA, Japan and China require improved energy efficiency.
A hyper-fast 20ns reverse-recovery time reduces PFC MOSFET switching losses, increases switching speed and improves energy efficiency, while a very fast soft recovery capability ensures ringing and EMI interference are reduced. Boost diode recovery losses are minimized by a low 3.9A reverse-recovery current, which also reduces power dissipation in the MOSFET and lowers the risk of system failure. A low 1.95V forward voltage drop also minimizes boost diode conduction losses.
Aimed at designers of PFC circuits who need to achieve the lowest possible energy losses, the DSR8F600 provides best-in-class performance, generating the least noise and achieving the highest power efficiency. The DSR8F600 is the first of a family of hyper-fast rectifiers; future introductions will provide even higher voltages and currents.
The DSR8F600 is available in the space-saving TSOT26 package. Further information is available at www.diodes.com.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor's SmallCap 600 and Russell 3000 Index company, is a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets. Diodes serves the consumer electronics, computing, communications, industrial, and automotive markets. Diodes' products include diodes, rectifiers, transistors, MOSFETs, protection devices, functional specific arrays, single gate logic, amplifiers and comparators, Hall-effect and temperature sensors; power management devices, including LED drivers, AC-DC converters and controllers, DC-DC switching and linear voltage regulators, and voltage references along with special function devices, such as USB power switches, load switches, voltage supervisors, and motor controllers. Diodes’ corporate headquarters and Americas' sales office are located in Plano, Texas. Design, marketing, and engineering centers are located in Plano; San Jose, California; Taipei, Taiwan; Manchester, England; and Neuhaus, Germany. Diodes’ wafer fabrication facilities are located in Kansas City, Missouri and Manchester, with two additional facilities located in Shanghai, China. Diodes has assembly and test facilities located in Shanghai and in Chengdu, China, as well as in Neuhaus and in Taipei. Additional engineering, sales, warehouse, and logistics offices are located in Taipei; Hong Kong; Manchester; Shanghai; Shenzhen, China; Seongnam-si, South Korea; and Munich, Germany, with support offices throughout the world. For further information including SEC filings, visit Diodes’ website at www.diodes.com.
###
Company Contact:
Diodes Incorporated
Francis Tang
VP, Worldwide Discrete Products