Diodes Incorporated — Analog and discrete power solutions

Protect Vehicle ECUs Against Reverse-Battery Connections with Automotive MOSFETs from Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the DMP4015SPSQ 40V P-channel MOSFET. This device is designed to protect automotive Electronic Control Units (ECUs) against the risk of reverse-battery connection. ECUs are used in a growing number of automotive control applications and, with some vehicles deploying up to 80 ECUs, the need to protect each one demands a simple and cost-effective solution, which this MOSFET provides.

The DMP4015SPSQ MOSFET acts as an ideal diode, allowing current to flow when the battery is correctly connected and blocking the current when the battery is accidentally connected in the reverse direction. Driving this device only requires a minimal number of passive components. By comparison N-channel MOSFETs require a charge pump to provide the gate drive voltage, adding complexity, cost and component count. Eliminating the switching topology of a charge pump also avoids issues with EMI emissions.

The avalanche rugged DMP4015SPSQ is 100% unclamped-inductive switch (UIS) tested to ensure the MOSFET will withstand the worst-case ISO7637 energy pulse that would occur if the supply was disconnected while powering an inductive load. The low RDS(on) of the DMP4015SPSQ, less than 11mΩ, ensures that power loss is minimized, resulting in lower temperature operation; this eases thermal design considerations and improves reliability. The parallel configuration of several MOSFETs can further reduce power losses, by a factor of n2.
The DMP4015SPSQ is offered in a PowerDI®5060 package and also available for the same application, are the DMP4015SK3Q in the TO252 (DPAK) package and DMP4015SSSQ in the SO-8 package. For further information, visit the Company’s website at www.diodes.com.

###
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
PowerDI is a registered trademark of Diodes Incorporated.

Related Files