Diodes Incorporated — Analog and discrete power solutions

Ultra-Compact TVS from Diodes Incorporated Provides Protection for USB 3.1/3.2 and Thunderbolt 3 Interfaces

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today announced its most advanced dataline transient voltage suppressor (TVS) ever, the DESD3V3Z1BCSF. Designed to provide exceptional TVS/ESD protection to the high-speed input/output ports of advanced systems-on-chips (SoCs) featuring differential signal line running at 5 GHz and beyond, the DESD3V3Z1BCSF-7 is indispensable for high-speed interfaces like USB 3.1/3.2, Thunderbolt™ 3, PCI Express® 3.0/4.0, HDMI 2.0a, and DisplayPort™ 1.4.

Modern SoCs are typically manufactured on advanced CMOS process nodes, which can make them more susceptible to transient voltages and electro-static discharges appearing at the input/output ports. Due to the higher than desired input channel capacitance, traditional TVS devices can degrade high-speed signals as they travel between connectors at the boundary of the adopting system and the input/output ports of SoCs. The DESD3V3Z1BCSF-7 has been developed using Diodes’ advanced in-house processes to achieve ultra-low input channel capacitance (0.175pF typical), low dynamic resistance, low trigger/holding/clamping voltages, and is assembled in a state-of-the-art package with ultra-low capacitance. Meticulous design results in exceptionally low insertion loss, meeting the signal integrity requirement of high-speed interface standards like USB 3.1/3.2 and Thunderbolt 3.

“As advanced interfaces like USB Type-C become widely adopted, protecting the ports of advanced SoCs with multi-gigahertz bandwidth will become more imperative. To ensure reliable operation of these SoCs and the USB Type-C ports, the need for an incredibly low profile TVS able to provide a high level of protection without impacting the integrity of the high-speed signals is now paramount,” commented Dr. Timothy Chen, Division Director, Diodes Incorporated.

In addition to its ultra-low input capacitance, the DESD3V3Z1BCSF-7 offers exceptional ESD protection that meets IEC61000-4-2 requirements of up to 8kV air and contact. It leads the industry by offering the best combination of clamping voltage (VCL = 4.5V typical for IPP = 3A), breakdown voltage (VBR = 9V maximum), and reverse standoff voltage (VRWM = 3.3V maximum), while peak-pulse power dissipation (PPP) is 25W over the short-circuit waveform of 8/20µs.

The DESD3V3Z1BCSF-7 is supplied in the ultra-compact chip-scale X2-DSN0603-2 package, measuring just 0.6mm x 0.3mm and only 0.3mm high, and is priced at $0.056 each for a 10k reeled quantity. Further information is available at www.diodes.com.

Thunderbolt is a trademark of Intel Corporation or its subsidiaries in the U.S. and/or other countries.
PCIe is a registered trademark of PCI-SIG.
DisplayPort is a trademark owned by the Video Electronics Standards Association in the United States and other countries.

Related Files