Diodes Incorporated — Analog and discrete power solutions

Automotive-Compliant Dual MOSFETs from Diodes Incorporated Minimize Power Losses to Deliver Cost-Effective High Efficiency Solutions

Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic, analog and mixed-signal semiconductor markets, today introduced the DMNH4015SSDQ and DMTH6016LSDQ. Featuring low figure-of-merit on-resistance and gate charge specifications, these latest 40V and 60V dual, co-packaged enhancement mode MOSFETs minimize power losses, enabling cost-effective, high-efficiency, automotive-compliant power management solutions. Targeted at synchronous rectification applications in automotive instrumentation clusters, head-up displays, and infotainment, navigation and driver assistance systems, the DMNH4015SSDQ and DMTH6016LSDQ are qualified to AEC-Q101 Rev-D standard for high reliability and supported by a PPAP (production part approval process).

When coupled with a PWM control IC, these dual MOSFETs are capable of creating highly efficient and cost-effective DC-DC converters. For example, when switched at 400kHz, the 60V DMTH6016LSD delivers a 5V output at a load current of 2A, while achieving an efficiency of 95%. Similarly, the 40V DMNH4015SSDQ delivers 5V at 2A with an efficiency of 91%.

Both devices are 100% avalanche rated to withstand the high pulse energy that can result from inductive loads, and are specified with a maximum junction temperature of +175°C for operation in high ambient-temperature environments.

The DMNH4015SSDQ and DMTH6016LSDQ are supplied in the standard, space-saving SO-8 package. For further information, visit the Company’s website at www.diodes.com.

Related Files