Diodes Incorporated — Analog and discrete power solutions

Tag: Automotive

Improving the Thermal Performance of BLDC Motor Controllers in Automotive Applications

Brushless direct-current (BLDC) motors are efficient, can operate at high speeds, and are easy to control. Hence they are becoming increasingly popular in automotive applications, including anti-lock braking systems (ABS), power steering, and electric and hybrid vehicles.

Read More

Understanding EMI Allows Designers to Make an Informed Decision When Selecting a Switching Converter for Automotive Applications

This article reviews the source and types of EMI in switching converters before explaining the differences between the regulatory standards for products in the industrial and automotive markets. Finally, it shows the techniques used by Diodes Incorporated to enable one of its DC-DC switching converters to comply with stringent automotive standards.

Read More

Understanding the Demands on Hall Sensors for Automotive Applications

The demand for compact, accurate position sensors in automotive applications will grow substantially to $1.6 billion by 2026, in line with the growth in electric vehicles (Figure 1). These sensors track the rotor’s position inside the motor responsible for traction, power steering, and windows; ensuring control and safety coverage.

Read More

New Advances in LED Control Systems for Automotive Exterior Lighting

The automotive lighting market continues to grow strongly and is forecast by analyst Yolé to reach US$38.8 billion by 2024. Over the past few years, LEDs have taken an increasing share of this market, and LED exterior lights have become a familiar sight on our roads. 

Read More

汽車應用中新增瞬態電壓抑制功能

In automotive applications, it’s essential to protect sensitive semiconductor components against power surges, transients and electrostatic discharge (ESD). A single transient voltage spike could easily damage or disrupt a component, while electrical noise of even relatively low energy can cause significant interruption to digital communications.

Read More

Selecting the Right MOSFETs for Motor Drive Applications

Automotive OEMs are migrating to BLDCs in order to maximize efficiency and reliability. This article looks at the important parameters engineers should consider during the design process, in order to meet these objectives.

Read More

Protecting Vehicle Electronics from Reverse-Battery Connection

During the life of the vehicle, its battery may need to be disconnected for maintenance work or to replace it if it has developed a fault. During reconnection it is possible to reverse the polarity of the battery connection, which can result in potential short-circuits and other problems with loads connected to the battery.

Read More

PCI Express Passes Other Standards Found in Automobile Entertainment Systems

Move over CANbus, PCI Express is the latest communications technology found in automotive infotainment.

Read More

LED Control Maximizes Benefits of Daylight Running Lamps

Daylight running lamps for motor vehicles are now a legal requirement in Europe. They became mandatory for new cars manufactured from February 2011 and for commercial vehicles from August 2012. Although they now need to be incorporated in vehicles by law, the daylight running lamp provides a number of opportunities for car and van designers to improve multiple aspects of the driving experience and their own brand image.

Read More

Self-Protecting MOSFETs Deliver Improved Reliability in the Harsh Environment of Automotive Applications

While it’s been said many times before, the automotive electrical environment is tough! As demonstrated in figure 1, the nominal battery voltage of an automobile can vary from -12V DC, under reverse battery condition, to +125V DC due to load transients and inductive field decay. Factor in wide variations in operating temperature, numerous interconnections and an open environment that is subject to possible ESD damage from human interactions, and you have an operating environment that is far more challenging than, for example, that of the consumer market segment.

Read More