Diodes Incorporated — Analog and discrete power solutions

Category: Automotive Applications

AH332 52xQ Image

Accurate Proximity Detection in Automotive Applications From Hall Effect Switches

As vehicles and their technology features become more sophisticated, Hall effect switches help make driving easier, safer, and more comfortable.

Read More
DIB073D2 PI3USB31532Q blog image

Simplifying In-Car Connectivity for High-Definition Video Over USB Type-C® and DisplayPort™

As modern-day vehicles are full of technology, automotive manufacturers are under pressure to provide high-definition screens for streaming video, games, and video calls to meet consumer expectations.

Read More
DIO 9964 FE FT Blog montage

New Two-Pad Crystal Uses Seam Sealing for Pb-Free, RoHS-Compliant Devices

The FE/FEQ & FT/FTQ families are RoHS-compliant two-pad crystals that use seam sealing, which makes them fully lead-free in contrast to equivalent crystals that use a glass-sealed design.

Read More
ZXMS82xxxS14PQ PR Image

How Intelligent MOSFET Switches Are Replacing Automotive Fuses and Relays

The automotive industry's rapid transition to electric or hybrid vehicles, and increasing ADAS and ECU usage, result in more power and computational performance being required to drive new loads and process data in real time.

Read More
DMTH4M70SPGWQ

40V MOSFET Delivers Efficiency Gains for Electric Vehicles

Right now, the automotive industry is going through a big transformation as it rapidly shifts from internal combustion engines to battery-powered electric vehicles (EVs).

Read More
AS2376Q Product Image

Precision Op Amps Handle Automotive Signal Conditioning Demands

It’s become commonplace to think of cars as computers on wheels—with many high-profile industry figures using such terminology. But that can be a misleading comparison, as analog signals are just as important as digital computing in the automotive industry.

Read More
Blog page thumbnail Harnessing PCIe 3.0 for In Vehicle High Speed Connections

Harnessing PCIe® 3.0 For In-Vehicle High-Speed Connections

As cars increasingly add new electronic capabilities and applications (such as advanced driver assistance systems (ADAS), intelligent cockpits, telematics, and infotainment), the in-vehicle systems must keep up.

Read More
Blog page thumbnail Small Efficient PoL Converters for Automotive Applications

Small, Efficient PoL Converters for Automotive Applications

As today’s cars are putting more and more demands on their electrical power systems, they must achieve high efficiency to reduce heat dissipation and cut electricity consumption. At the same time, they need to be small enough to fit wherever needed, with suitable performance and flexibility.

Read More

Brushed Motors Are Not Going Away

Even when not taking into account the electrification of the drivetrain, the number of electric motors in the average car is increasing significantly.

Read More
Meeting automotive requirements for PoL Converters

Meeting Automotive Requirements for PoL Converters

Today’s cars are computers on wheels: full of complex electronics which all must be powered. Nowadays, modern cars include at least 150 electronic control units (ECUs).

Read More

1 2