Diodes Incorporated — Analog and discrete power solutions

技術文章

Designing a Gate Driver Circuit to Achieve Optimum Switching Performance in a Full-Bridge DC-DC Converter

This article discusses critical design techniques and layout parameters when using the DGD2190M gate driver ICs, which drives each half of the primary side in a full-bridge switching converter.

Read More

Battery-Discharge Protection for Appliances on the Move

Using a MOSFET as an ideal diode can provide robust and reliable safety protection for the emerging generation of autonomous appliances.

Read More

Improving the Thermal Performance of BLDC Motor Controllers in Automotive Applications

Brushless direct-current (BLDC) motors are efficient, can operate at high speeds, and are easy to control. Hence they are becoming increasingly popular in automotive applications, including anti-lock braking systems (ABS), power steering, and electric and hybrid vehicles.

Read More

Understanding EMI Allows Designers to Make an Informed Decision When Selecting a Switching Converter for Automotive Applications

This article reviews the source and types of EMI in switching converters before explaining the differences between the regulatory standards for products in the industrial and automotive markets. Finally, it shows the techniques used by Diodes Incorporated to enable one of its DC-DC switching converters to comply with stringent automotive standards.

Read More

Three Steps to Minimize Jitter in Gbps System Designs

The challenge of clock jitter—which adversely impacts high-speed protocols such as Ethernet, PCI Express®, and USB 3.0—is becoming more significant as next-generation protocols look to deliver data rates at hundreds of gigabits per second (Gbps). Understanding three key points can help you achieve success against jitter in your next design.

Read More

Understanding the Demands on Hall Sensors for Automotive Applications

The demand for compact, accurate position sensors in automotive applications will grow substantially to $1.6 billion by 2026, in line with the growth in electric vehicles (Figure 1). These sensors track the rotor’s position inside the motor responsible for traction, power steering, and windows; ensuring control and safety coverage.

Read More

Simplify Your Embedded Designs Using I²C I/O Expanders

The I²C two-wire bus is still as popular today as when Philips originally invented it in 1982. Initially operating at 100KHz, the latest incarnation, version 7 (2021) Ultra-Fast-mode (UFm), now clocks at 5MHz—making it fast enough for most medium-speed peripherals, including digital I/O, GPIO, keyboards, keypads, and sensors.

Read More

Use a ReDriver™ or ReTimer for Longer and Thinner USB, USB Type-C, and DP Cables

USB, USB Type-C®, and DisplayPort™ (DP) cables have become so ubiquitous as to even be purchased in low-cost convenience stores. However, while two individual cables may appear identical to the naked eye, they can differ considerably in the quality of performance they provide. Low cost can mean low quality, and alongside instances where cheap cables have caused electronic equipment to malfunction or have corrupted data, they typically cause poor picture quality or slow down the rate of data transfer to well below the multi-gigabit bandwidth offered by the latest USB specification (USB 4).

Read More

Plug-and-Play USB Charging Controller Makes Charging of Battery-Powered Devices Seamless

In the not-too-distant past, it seemed like every electronic device had its own custom power supply, cable, and interface (Figure 1). USB Type-C® (or USB-C®), which implements the USB power delivery (USB-PD) specification, was supposed to solve this problem by introducing a single standard interface that all devices could use.

Read More
PI7C9X3G606GPB

Advanced PCIe Features for Power-Conscious and Mission-Critical Applications

Today’s PCIe 3.0 switches, which support data speeds up to 8GT/s per lane, combine generous bandwidth and up-to-the-minute power-management and RAS features to meet the needs of mobile and embedded applications.

Read More

1 2 3 4