Diodes Incorporated — Analog and discrete power solutions

PCIe 3.0 Packet Switch from Diodes Incorporated Offers Fan-Out and Multi-Host Capabilities

Diodes Incorporated (Diodes) (Nasdaq: DIOD) is introducing its latest PCIe® 3.0 packet switch, the DIODES™ PI7C9X3G1224GP. A high-performance 12-port, 24-lane device, it can be used in edge computing, data storage, communications infrastructure, and  incorporated into host bus adaptors (HBAs), industrial controllers, and network routers.

The PI7C9X3G1224GP has a low packet forwarding latency of less than 150ns (typical). Flexible port configuration of this device is achieved by having scope to allocate variable lane widths to each of its ports. For fan-out purposes, any port of the packet switch can be configured as upstream and connected to multiple downstream ports. Through cross-domain end-point (CDEP) configuration of certain ports, it is possible for multi-host arrangements to be supported - leading to boosted performance and expanded functionality. The adaptive receive side and transmit side equalization (RXEQ/TXEQ) features included assist with maintaining signal integrity levels and ensuring continued system stability.

The integrated PCIe 3.0 clock buffer is another plus point of the PI7C9X3G1224GP. This simplifies designs and reduces the overall bill-of-materials (BOM) costs. Advanced power management capabilities make it highly suited to system designs where energy saving gains are important. The operational temperature is continuously monitored using its built-in thermal sensor. Error reporting and other diagnostic functions are also included.

The PI7C9X3G1224GP is supplied in a 324-pin flip-chip BGA package format, and it is available at $56.47 in 1000 piece quantities.

 

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.

 

The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.

DIODES™ is a trademark of Diodes Incorporated in the United States and other countries.

All other trademarks are the property of their respective owners.

 

Company Contact:                                   Investor Relations Contact:

Diodes Incorporated                                 Shelton Group

Emily Yang                                                   Leanne K. Sievers

SVP, Worldwide Sales and Marketing     President

P: 972-987-3900                                         P: 949-224-3874

Contact Us                                                   E: lsievers@sheltongroup.com

Related Files