Diodes Incorporated (Nasdaq: DIOD), a leading global manufacturer and supplier of high-quality application specific standard products within the broad discrete, logic and analog semiconductor markets, today introduced the AP3785T. This AC-DC primary-side switched-mode power supply controller is aimed at 8W to 15W 5V output USB chargers that necessitate ultra-low standby power. This market requirement is driven by smart phones and tablets with larger battery capacities and increasingly tight power supply efficiency regulations.
Various features contribute to the superior performance delivered by the AP3785T: a no-load input power rating of less than 10mW meets the standby criteria for ‘Super Star’ chargers; higher efficiency and better EMI result from valley-on operation and a low VCS jitter specification; higher conversion efficiency is also achieved when the AP3785T is used in conjunction with a synchronous rectifier, such as the AP4341. Multiple PWM/PFM control modes further help improve audio noise and efficiency.
Over-voltage protection, output short-circuit protection and transformer saturation protection (via primary peak-current limitation) are all built into the AP3785T. Internal temperature protection is also provided along with a dedicated pin to support external temperature protection. When operating as a constant current regulator, a feedback pin enables compensation for changes in line voltage whereas in constant voltage mode the AP3785T can compensate for voltage drops due to different cable lengths or gauge.
The AP3785T is offered in a small, standard pinout SO-8 package. Further information is available at www.diodes.com.
###
Company Contact:
Diodes Incorporated
Julie Holland
VP, Worldwide Analog Products
P: 972-987-3900
E: pressinquiries@diodes.com
Investor Relations Contact:
Shelton Group
Leanne K. Sievers
EVP, Investor Relations
P: 949-224-3874
E: lsievers@sheltongroup.com