Diodes Incorporated — Analog and discrete power solutions

20Gbps ReDrivers from Diodes Incorporated Combine Superior Signal Integrity Capabilities with Low Power Operation

Diodes Incorporated (Diodes) (Nasdaq: DIOD) has announced further additions to its extensive range of programmable multi-channel linear ReDrivers™, releasing three new 20Gbps devices with 1.8V voltage ratings addressing fast growing USB4® Gen3, Thunderbolt™ 4.0 and DisplayPort 2.0 standards. The DIODES™ ReDrivers™ PI2DPX2020, PI2DPX2023, and PI2DPX2063 are targeted at use in laptops, desktop PCs, workstations, active cables, monitors and docking applications. Their low power consumption and compact, low-profile packaging also makes them highly optimized for tablets and notebook computers.

Each of the new linear ReDrivers allows flexible adjustment of signal integrity parameters, such as equalizer and flat gain, through the various settings available. This mitigates channel loss and extends reach. These devices are transparent to channel link training. In addition, they exhibit ultra-low latency figures (<300ps).

The PI2DPX2020 supports different operational modes for maximum design-in flexibility. These are 20Gbps/40Gbps USB4 Gen3 (x1/x2), 20.625Gbps/41.25Gbps Thunderbolt 4.0 (x1/x2), 10Gbps/20Gbps USB4 Gen 2 (x1/x2), 20Gbps USB4 Gen2/2 lanes of DisplayPort 2.0 and 4 lanes of DisplayPort 2.0. The 4-lane PI2DPX2023 20Gbps DisplayPort 2.0 (UHBR20) ReDriver supports pin strap equalizer and gain parameter control, while for the PI2DPX2063 20Gbps DisplayPort 2.0 (UHBR20), this is achieved via the I2C interface pin.

These new ReDrivers have auto power-saving modes built in. They are supplied in 32-pin W-LGA4528 packages (with 2.85mm x 4.5mm x 0.7mm dimensions) and support an industrial temperature range.

In 5000 piece quantities, the PI2DPX2020 is available at $2.99, the PI2DPX2023 is available at $3.00, and the PI2DPX2063 is available at $2.95.

 

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.

 

The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.

DIODES and ReDriver are trademarks of Diodes Incorporated in the United States and other countries.

All other trademarks are the property of their respective owners.

 

Company Contact:                                   Investor Relations Contact:

Diodes Incorporated                                 Shelton Group

Emily Yang                                                   Leanne K. Sievers

SVP, Worldwide Sales and Marketing     President

P: 972-987-3900                                         P: 949-224-3874

Contact Us                                                  E: lsievers@sheltongroup.com

Related Files