Diodes Incorporated (Nasdaq: DIOD) has introduced the AP7347DQ low dropout (LDO) voltage regulator, which is highly optimized for demanding noise-sensitive power-related automotive applications. This automotive-compliant high output accuracy LDO is AEC-Q100 Grade 1 qualified, manufactured in IATF 16949 certified facilities, and fully supports automotive production part approval processes (PPAPs). These qualities make it well-suited to design in to a range of key in-vehicle functions, including point-of-load (POL) applications in ADAS, automotive wireless communication systems, RF subsystems, and infotainment power sources.
A 75dB power supply rejection ratio (PSRR), combined with an output noise of just 60µVrms, gives the AP7347DQ considerable performance advantages. It is available in 12 fixed output voltage variants with a ±1% voltage-output accuracy, which is maintained across its entire -40°C to 125°C operational temperature range. Its 1.7V to 5.5V wide input voltage range gives it the versatility to address numerous automotive application requirements, while its 60µA quiescent current mitigates standby power losses.
The AP7347DQ has an enable pin; a built-in active discharge function ensures that the system starts up in a known state if the device has been disabled. Overtemperature and short-circuit protection are integrated, incorporating a 180mA foldback current limit should a short circuit occur.
The AP7347DQ is available in SOT25 and high-power density sidewall plated W‑DFN2020‑6 (SWP) packages. It has a $0.27 unit pricing in 1000 piece quantities.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 31 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.Diodes.com.
Company Contact: Investor Relations Contact:
Diodes Incorporated Shelton Group
Emily Yang Leanne K. Sievers
SVP, Worldwide Sales and Marketing EVP, Investor Relations
P: 972-987-3900 P: 949-224-3874
Contact Us E: lsievers@sheltongroup.com