Diodes Incorporated (Diodes) (Nasdaq: DIOD) today announced the release of its first Silicon Carbide (SiC) Schottky barrier diodes (SBD). The portfolio includes the DIODES™ DSCxxA065 series with eleven products rated at 650V (4A, 6A, 8A, and 10A) and the DIODES™ DSCxx120 series with eight products rated at 1200V (2A, 5A, and 10A).
These wide-bandgap SBDs bring the benefits of significantly improved efficiency and high-temperature reliability, while also responding to market demands for reduced system running costs and low maintenance. The devices are suitable for AC-DC, DC-DC, and DC-AC switching converters, photovoltaic inverters, uninterruptable power supplies, and industrial motor drive applications. These devices can also be used in a variety of other circuits, such as boost converters for power factor correction.
The efficient performance of these SiC devices are superior to those of conventional silicon-based products, and provide power supply designers with uncompromising product performance benefits, such as:
Three package options include surface mount TO252-2 (Type WX), through-hole TO220AC (Type WX), and ITO220AC (Type WX-NC).
The DSCxxA065 and DSCxx120 series are available from $1.24 to $2.33 and $1.70 to $6.68 respectively in 1,000 piece quantities.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information, visit www.diodes.com.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
DIODES is a trademark of Diodes Incorporated in the United States and other countries.
All other trademarks are the property of their respective owners.
Company Contact: Investor Relations Contact:
Diodes Incorporated Shelton Group
Emily Yang Leanne K. Sievers
SVP, Worldwide Sales and Marketing President
P: 972-987-3900 P: 949-224-3874
Contact Us E: lsievers@sheltongroup.com