Diodes Incorporated (Diodes) (Nasdaq: DIOD) has introduced the DIODES™ ZXMS81045SPQ, its first protected, automotive-compliant, high-side IntelliFET®. This device is capable of delivering high power from a small footprint, while also providing protection and diagnostic capabilities. It is suitable for driving 12V automotive loads, such as LEDs, bulbs, actuators, and motors in automotive body control and lighting systems.
The ZXMS81045SPQ features a 41V-rated N-channel FET with onboard circuitry that provides protection against short circuits, manages inrush currents, and safeguards against overvoltage conditions including load dumps. In addition, the ZXMS81045SPQ also features overtemperature protection with auto-restart, plus protection against electro-static discharges (ESD). Loss of ground and reverse polarity protection can also be implemented with the aid of a few external components.
A dedicated current sense (IS) pin provides precision analog current monitoring of the output and fault indication for short to battery; short to ground and open load detection.
The ZXMS81045SPQ provides an efficient, reliable, smaller footprint alternative to relays, fuses, and discrete circuits. It is also a form, fit, and functional equivalent for existing power switch devices, where customers need improved product supply.
The ZXMS81045SPQ is qualified to AEC-Q100, PPAP capable, and manufactured in IATF 16949 certified facilities. It is supplied in a SO-8EP package and is available at $0.95 in 2,500 piece quantities.
About Diodes Incorporated
Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 32 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com.
The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.
DIODES is a trademark of Diodes Incorporated in the United States and other countries.
IntelliFET is a registered trademark of Diodes Incorporated in the United Kingdom and other countries.
Company Contact: Investor Relations Contact:
Diodes Incorporated Shelton Group
Emily Yang Leanne K. Sievers
SVP, Worldwide Sales and Marketing President
P: 972-987-3900 P: 949-224-3874
Contact Us E: lsievers@sheltongroup.com