Diodes Incorporated — Analog and discrete power solutions

Low Standby Power, Non-Isolated Offline Switcher from Diodes Incorporated Significantly Reduces BOM Costs

Diodes Incorporated (DIODES™) (Nasdaq: DIOD) has introduced a universal AC high-voltage input non-isolated offline switcher IC to further strengthen its power products portfolio. The AP3928 addresses the challenges associated with using a bias power supply. It delivers safe and reliable power, while simultaneously maintaining elevated performance figures and enabling significant cost savings. This switcher IC is optimized for situations where higher power levels are mandated, such as in industrial control or home automation systems, home appliances, and IoT devices.

The AP3928 has a 600mA maximum output current that allows for a 10W output power rating. A key differentiator of this high-voltage switcher IC is that it supports conventional offline non-isolated flyback configurations, as well as more streamlined non-isolated buck configurations, keeping the bill-of-materials (BOM) spend to a minimum.

The peak current and switching frequency will continuously reduce as the load decreases, meaning that this device can achieve heightened degrees of efficiency in light load conditions. It is thereby well-suited for any form of equipment that spends prolonged time in sleep mode.

The AP3928’s low standby power of less than 30mW is another important attribute. This is of particular value in small domestic appliances and IoT devices, where available battery power needs to be conserved.

The DIODES AP3928 switcher IC is supplied in a compact SO-8 package. To ensure safety, it meets high-voltage creepage requirements, and can support operational junction temperatures reaching up to +150°C. Overtemperature, output short, overload and open-loop protection functions are all included, as well as undervoltage lockout. The AP3928 is available at $0.25 in 1000 piece quantities.

 

DIODES is a trademark of Diodes Incorporated in the United States and other countries.

 

The DIODES logo is a registered trademark of Diodes Incorporated in the United States and other countries.

 

About Diodes Incorporated

Diodes Incorporated (Nasdaq: DIOD), a Standard and Poor’s SmallCap 600 and Russell 3000 Index company, delivers high-quality semiconductor products to the world’s leading companies in the consumer electronics, computing, communications, industrial, and automotive markets. We leverage our expanded product portfolio of discrete, analog, and mixed-signal products and leading-edge packaging technology to meet customers’ needs. Our broad range of application-specific solutions and solutions-focused sales, coupled with worldwide operations of 31 sites, including engineering, testing, manufacturing, and customer service, enables us to be a premier provider for high-volume, high-growth markets. For more information visit www.diodes.com

.

 

Company Contact:                                   Investor Relations Contact:

Diodes Incorporated                                 Shelton Group

Emily Yang                                                   Leanne K. Sievers

SVP, Worldwide Sales and Marketing      President

P: 972-987-3900                                          P: 949-224-3874

Contact Us                                                   E: lsievers@sheltongroup.com

 

 

Related Files