Diodes Incorporated — Analog and discrete power solutions
Back to 觀點

How Multi-Channel LED Driver Technology is Revolutionizing the Way We Illuminate Spaces and Convey Information New Post

AL58221 blog image

By Peter Chan, LED Lighting Application Manager

 

 

Architectural lighting has been transformed with the ability to create dynamic facades that change color and pattern, enhancing the night-time skyline and celebrating special occasions with bespoke light shows. Public spaces have become more interactive and informative with digital signage providing real-time updates, wayfinding solutions aiding transportation hubs, and museums utilizing LED screens to create immersive educational experiences.

Stadiums and arenas have also seen a significant upgrade, with colossal LED screens offering instant replays and close-up action to enhance the spectator experience. Moreover, the advent of digital billboards has revolutionized outdoor advertising, allowing for flexible and dynamic content that can be updated with ease to capture the attention of passersby.

One of the most significant trends is the push towards creating displays with dynamic patterns and interactive information with exceptional brightness and color uniformity. Achieving this uniformity is a complex task, especially as displays become larger and more intricate. Another focus for design engineers is on improving thermal management and reducing power consumption to create more reliable, sustainable, and cost-effective systems.

Maintaining signal integrity over long cable runs is also essential for these large installations, where the distance between the LED driver and the LEDs can be considerable. Additionally, as LED systems become more widespread, the need to minimize electromagnetic interference (EMI) grows more pressing to ensure compliance with strict regulatory standards and to prevent disruption to other electronic devices.

Finally, the human eye is sensitive to rapid fluctuations in light output, particularly at low frequencies. Flicker can lead to discomfort and eye strain and, in severe cases, can trigger photosensitive epileptic seizures. The IEEE Standard for Modulating Current in High-Brightness LEDs for Mitigating Health Risks to Viewers, known as the IEEE 1789-2015 standard, provides a comprehensive set of recommendations for minimizing flicker.

Against this backdrop of regulatory requirements and health considerations, Diodes Incorporated (Diodes) has introduced the AL58221, a 12-channel linear LED driver with three external resistors to set independent RGB currents. Its high-accuracy current sink with channel-to-channel and device-to-device current matching ensures uniform brightness and color across LED displays. This precision is crucial for maintaining visual quality, particularly in high-definition applications where any deviation can be noticeable and detrimental to the viewer experience.

The driver's adaptive pulse density modulation (APDM) technique helps mitigate non-ideal IOUT distortion to spread out the current distribution to reduce EMI and increase visual refresh rates for enhanced performance. By achieving refresh rates of >1,000Hz at 16-bit and >256kHz at 8-bit grayscale, the device helps minimize flicker, aligning with the stringent demands of regulatory standards and enhancing viewer comfort.

The LED driver’s capabilities extend beyond flicker reduction. Its output-current bilateral processing helps to minimize EMI. Scalability is another feature of the device, which can cascade (daisy-chain) up to 1,030 devices in digital serial interface through the microprocessor (MCU). This feature simplifies the design and deployment of large-scale architectural installations or expansive digital billboards without the need for complex wiring or additional components.

By optimizing power usage, the driver contributes to reduced energy consumption and operating costs, aligning with the industry's move toward sustainability. Effective thermal management also ensures the longevity and reliability of LED systems, which is paramount for maintaining performance over time and minimizing maintenance costs.

The AL58221 LED driver enables system design engineers to meet energy-efficiency demands, visual excellence, and regulatory compliance. With its capacity to ensure uniform brightness, minimize flicker, and reduce EMI, this driver enables superior performance for architectural lighting, digital signage, and displays.

 
 
 

The Diodes logo is a registered trademark of Diodes Incorporated in the United States and other countries.

All trademarks are the property of their respective owners.

© 2025 Diodes Incorporated. All Rights Reserved.